Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What does the small C mean in the upper right corner of the LTMCU display for TeSys T controller?
Issue:
Troubleshooting C Status on LTMCU Display for TeSys T Controller

Product Line:
TeSys T, LTMCU, LTMR

Environment:
All

Resolution:



When you are in system config mode, you will see a small "c" in upper right corner of LTMCU.  This would mean that the unit can be programmed.  This also means that the unit cannot be commanded to run unless the system is out of configuration mode.

To adjust this status mode from the keypad.
  • Arrow down to services and enter.
  • Arrow down to config and enter.
  • Press enter on end config.
  • Arrow down to yes and enter.
  • This will now hide the C on top right corner which confirms that you are no longer in config mode.