Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I convert ATV32 programming to ATV320 programming using a Multiloader and SoMove?
Issue:
ATV32 programming conversion to ATV320 programming using a Multiloader and SoMove

Product Line:
Altivar 32, Altivar 320, SoMove, Multiloader

Environment:
All

Cause:
Need to transfer programming from ATV32 to ATV320

Resolution:
Please refer to the attached document which details this procedure.

Schneider Electric Saudi Arabia

Attachment(s)
converting atv32 CFG to atv320.pdf [409.5 KB]