Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
140CRA31200 Product Robustness Improvement
Title
140CRA31200 Product Improvement

Issue
Hardware changes to 140CRA31200 to improve robustness

Product Line
Quantum, M580

Environment
Unity Pro, Control Expert

Resolution
The 140CRA31200 underwent a product robustness improvement (Hardware redesign). This improvement has been Verified & Validated and applied in production.
The Standard 140CRA31200 product version with the modification implemented is since PV05.