Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change the wiring settings and CT ratio on the Acti 9 iEM3255 kWh Meter
Enter the configuration by pressing the ESC and OK button on the front of the Meter simultaneously. Enter the Password "0010"

The first parameter is Wiring - Change? to enter press OK and change the wiring setting as per the connection and save.

The next parameter will be CT & VT Ratio - Change? To enter press OK, change the CT Secondary and Primary as per the ratio of connected CT.