Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Communication address do I write my speed reference to on the ATV340 drive?
Issue:
When controlling over the network, what address do I write my speed reference to on the ATV340 drive?

Product Line:
ATV340

Environment:
All models, All serial numbers

Cause:
NA

Resolution:
Address 8502 and 8602 are used to enter the speed reference.  If you are writing your speed reference in Hertz, use address 8502.  If you are writing your speed reference in RPM, use address 8602.   If using 8502, you will write the speed reference in tenths of Hertz.  Thus to enter a speed of 60.0Hz, you would write 600 to address 8502.