Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an averaging block for an analog signal?
Issue
Using Concept, Unity Pro or Control Expert is there a block that can be used for a moving average?

Product line
Concept, Unity Pro, Control Expert

Resolution
The AVGMV or AVGMV_K blocks could be used. They take in a REAL input and allow the user to define the number of scans that will buffer before averaging. If the analog signal is not REAL, use standard conversion blocks such as W_INT_REAL and REAL_TO_WORD.

These blocks are part of the included CONT_CTL library and not a library that needs to be installed separately.