OFS server version 3.61 shuts down after starting.
Issue
OFS server shuts down a few seconds after it starts.
Product Line
OFS version 3.61
Environment
Windows 10
Resolution
The OFS server shuts down a few seconds after it starts.
The reason why this occurs is due to OFS not being able to find the Temp folder. OFS needs to create a folder in the 'C:\Temp' folder.
If it cannot find the Temp folder, it will shut down.
To resolve the issue, create a 'Temp' folder in the 'C' drive of the PC..
OFS server shuts down a few seconds after it starts.
Product Line
OFS version 3.61
Environment
Windows 10
Resolution
The OFS server shuts down a few seconds after it starts.
The reason why this occurs is due to OFS not being able to find the Temp folder. OFS needs to create a folder in the 'C:\Temp' folder.
If it cannot find the Temp folder, it will shut down.
To resolve the issue, create a 'Temp' folder in the 'C' drive of the PC..
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.