Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV320 drives do they come with integrated Bluetooth communications?
Issue:
Bluetooth availability on the ATV320.

Product Line:
ATV320

Environment:
All

Cause:
Bluetooth

Resolution:
The ATV320 drives both Versions C and B do not have a built-in Bluetooth option.