Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause an bOF or brake resistor overload fault on the ATV630 and ATV930 Process drives?
Issue:
ATV630 and ATV930 causes with an bOF or brake resistor overload fault.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
Parameter setting of the braking resistor not correct (brtC, brV, brP)

Resolution:
Principle:
The thermal model of the braking resistor has detected and overload.The themal state of the BR can be monitored with the parameter tHb.

Probable cause:
- parameter setting of the braking resistor not correct (brtC, brV, brP)

Remedies:
- check the nominal power of the braking resistor.
- verify the BR parameters brP, brV, brtC
- check with SoMove service section the thermal states TH1R / TH2R / TH3R
- check the thermal state parameter tHb [Braking Resistor monitoring]