Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an brF or brake feedback fault on the ATV630 or ATV930 drives?
Issue:
ATV630 and ATV930 showing brF or brake feedback fault.

Product Line:
ATV630 or ATV930 drives

Environment:
All

Cause:
The monitoring of the brake (assign the braking contact to a logic input) does not
match the braking command.

Resolution:
brake feedback and the control circuit.
• Check the mechanical state of the brake.
• Check parameter BCI → brake contact input
• Check parameter BLC → brake assignment.
• Check parameter BRT → brake release time.
• Check parameter BET → brake engage time.