Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 32Q/40 - Directional reactive overpower?
Two-way protection based on calculated reactive power to detect field loss on synchronous machines:
  • reactive overpower protection for motors which consume more reactive power with field loss
  • reverse reactive overpower protection for generators which consume reactive power with field loss.