Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 32P - Directional active overpower?
Two-way protection based on calculated active power, for the following applications:
  • active overpower protection to detect overloads and allow load shedding
  • reverse active power protection:
  1. against generators running like motors when the generators consume active power
  2. against motors running like generators when the motors supply active power.