Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it necessary to provide 230V voltage to CL1, CL2 terminals for the ATS01N209QN?
ATS01N209QN does not use external supply for control circuit.
External supply is needed only for:
ATS01N1..FT (CL1 - CL2 or 24V)
ATS01N2..LY (terminals 6-7)