Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the content of PCSPEAV98949 spare fuses for Accusine Active Harmonic Filters?
The content is:

Fuse Description                 Rating         QTY per Kit            Active Filter Size            Replaces Fuse
UL Type CC Slow Blow        6A 600VAC       1                          60A, 120A                         F1
UL Type CC Slow Blow        9A 600VAC       1                         200A, 300A                        F1
UL Type CC Slow Blow        4A 600VAC       3                             All                              F2, F3, F4
UL“ Solar” Fuse                  12A 1000VDC    3                             All                              F5, F6, F7

All 4-9Amp fuses are CC ferrule 10.3x38.1, type KLDR x  or FNQ-R-x (x..Amps)
12A fuse 0090.0012 (Schurter) or 0SPF012.T (Litelfuse)