Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 27 - Undervoltage?
Protection of motors against voltage sags or detection of abnormally low network voltage to trigger automatic load shedding or source transfer.


Works with phase-to-phase voltage (Sepam series 20 and Sepam series 40) or phase-to-neutral voltage
(Sepam series 40 only), each voltage being monitored separately.