Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 64REF - Restricted earth fault differential?
Detection of phase-to-earth faults on 3-phase windings with earthed neutral, by
comparison of residual current calculated from the 3 phase currents and residual
current measured at the neutral point.

Characteristics
  • instantaneous tripping
  • percentage-based characteristic with fixed slope and adjustable low set point
  • more sensitive than transformer or machine differential protection.

Schneider Electric Saudi Arabia

Attachment(s)
ANSI 64REF.PNG.png [25.32 KB]