Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the speed pot cause my drive to run in reverse?
Issue:
Drive is running at Low Speed, or 0Hz when scaled to 100% and then runs up to 60Hz or High Speed when at 0%.

Product Line:
All Altivar drives

Environment:
All

Cause:
Incorrect wiring

Resolution:
For the drive to run forward, the Analog inputs are polarity sensitive.  The Output, or wiper contact from the drive needs to be on the analog input terminal.  If you are seeing the scaling when adjusting from 0-100% then you may just need to swap the +10 and COM wires to change the polarity.