Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
CANopen telegram. What is the content of CANopen data frame and its length?

CANopen data frame consists of :
SOF = start of frame (1 bit)
Arbitration field = 12 or 32 bits depending on whether 11 or 29 bit identifier is used (feature of the device)
Control field = 6 bits
Data field depends on mapping. Process data object can carry max 8 bytes. If each variable takes 2bytes then max content of 4 variables in data filed is possible.
CRC = control redundancy check (16 bits)
ACK = acknowledge (2 bits)
EOF = end of frame + intermission (7+3 bits)

Total: 47 bits + data filed (derived from number of variables mapped and their length).