Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION9000: Maximum number of option modules
Issue
Is there a maximum number of option modules that could be installed on ION9000 meter?

Product Line
ION9000

Environment
Digital/Analog Input/Output Option Modules

Cause
The optional I/O available on ION9000 and limitation.

Resolution
  • The maximum number of option modules supported by the device is four. However, there are limitations.
  • Depending on the type and quantity of option modules attached to your meter, you may need to reduce your meter’s maximum operating temperature or limit the number of option modules.
**Warning: EQUIPMENT DAMAGE CAN OCCUR. Do not exceed the maximum number of option modules. Failure to follow these instructions can result in equipment damage.**

The maximum operating temperature for option modules is as follows:
Maximum operating temperature
PM89M2600
Digital (2 out, 6 in)
PM89M0024
Analog (2 out, 4 in)
70 ºC (158 ºF)
0 - 4
0,1
70 ºC (158 ºF)
0
2
60 ºC (140 ºF)
1,2
2-4