Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the electrical endurance of switch units in SM6 36kV? how many times the switch can break its rated current "Ir"?
Switches used for load-breaking in SM6 36kV complies to electrical endurance class "E3" to IEC 62271-103,
The switch can break up to 100 breaks at its rated current (Ir) at a power factor of 0.7.