Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 37P - Directional active underpower?
Two-way protection based on calculated active power
Checking of active power flows:
  • to adapt the number of parallel sources to fit the network load power demand
  • to create an isolated system in an installation with its own generating unit.