Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 24 - Overfluxing (V/Hz)?
Protection which detects overfluxing of transformer or generator magnetic circuits by calculating the ratio
between the greatest phase-to-neutral or phase-to-phase voltage divided by the frequency.

Characteristics
  • machine coupling to be set up
  • definite time (DT) or IDMT time delays (choice of 3 curves).