Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I configure VD23 voltage detection relay? What are the setting ranges available?

Configuration of detection mode can be done via microswitches on the units' rear part,
the voltage configuration thresholds are as follows:
image 1