Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I find the number of requests serviced by the pocessor per mast cycle
Issue
How do I find the number of requests serviced by the pocessor per mast cycle.

Product Line
M580, M340

Environment
Unity, Control Expert.

Resolution
This can be accomplished by viewing the system word %SW87 value with an animation table.  This will provide the number of backplane requests being processed by the CPU per mast cycle.