Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the breaking principle for SF circuit breakers?
SF circuit breakers use the puffer principle with SF6 gas.
This methods cools and extinguishes the electrical arc as it passes through zero current by puffing a gas compressed by a piston attached to the moving contact. The gas is channeled by an insulating nozzle towards the tubular arcing contacts that are used as an exhaust.
The operating sequence in a puffer-type breaking chamber with the moving part actuated by a control mechanism is as follows:

1- The circuit breaker is closed.


2- Following an opening order the main contacts separate (a) and the current is directed into the breaking circuit (b).
When the main contacts start to open the piston (c) slightly compresses the SF6 gas in the compression chamber (d)




3- An electrical arc appears on separation of the arcing contacts. The piston (c) continues its travel downwards.
A small quantity of the gas channeled by the insulating nozzle (e) is injected towards the arc.
For low current breaking, the arc is cooled by forced ventilation. However, for high currents the thermal expansion moves the hot gases towards cooler parts in the breaking unit.
The distance between arcing contacts becomes sufficient to allow breaking of the current when it passes through zero due to the dielectric properties of the SF6 gas


4 The moving parts finish their movement and injection of cold gas continues until the contacts are fully open.
he circuit breaker is open


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre