Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video Altivar Process: How to connect to webserver?

Article available in these languages: Dutch

Altivar Process ATV600 or ATV900 have a Webserver embedded !
How to connect your computer to the Altivar to see the Webserver page on your browser ?
(Ethernet, WIFI, Bluetooth, IPV4,6 Modbus, PROFINET ….)

Description also to connect to Wifi with the WIFER option (TCSEGWB13FA0).



Related video: "Altivar Process: What are the Webserver's main features?"