Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does ‘Supply Monitoring’ affect over current detect?
Question:
As for the X80 DDO module,
does ‘Supply Monitoring’ affect over current detect? i.e. If I uncheck Supply Monitoring can I assume this channel will no longer trip on over current?

Answer:
No, supply monitoring is only used for supervising the threshold voltage of Pre-actuator. In case it does not exceed the threshold voltage, the output will be off.
The channel over current will be always indicated via LED

Schneider Electric Saudi Arabia

Attachment(s)
SupplyMonitoring.png [123.23 KB]