Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we feed BMXEHC module by the DC in/out of BMXCPS
Question:
Can we feed BMXEHC module by the DC in/out of BMXCPS?

Answer:
Yes, and it is recommended to use ‘DC out’ of BMXCPS(for ins.  BMXCPS2000) instead of ‘DC in’ of BMXCPS(for ins. BMXCPS3020) since ‘DC out’ has some off delay versus ‘DC in’ in case of CPS off, where
the current counter value could be timely saved.