Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between Pixel Resolution and Display Resolution?

Issue:
The datasheet describes Pixel resolution and Display resolution. What is the difference?

Product Line:
Magelis HMI,iPC

Resolution:
Pixel resolution and display resolution are two different things. The Pixel Resolution defines how detailed an individual pixel will appear on the screen.

The Pixel Resolution of the HMIDM9521 is 1024x1024.  The images would appear blurry say at 10 x 10 compared to the 1024 x 1024 on the same display resolution.

See these image below as an example.

The display resolution is what we commonly all work with that defines the Height and Width of the screen.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
Images.png [25.11 KB]