Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement part number for the MCB or Main Control Board for the ATV930 or ATV960 Drives?
Issue:
Part number for Main Control Board for ATV930/ATV960

Product Line:
ATV930 and ATV960 Drives

Environment:
All

Resolution:
The MCB or Main Control Board pat number for the ATV930, ATV980 or ATV960 drive is VX4B900100.
Note: This part can be ordered, however, be aware that this is not a standard part.
**For use in High HP ATV960 or ATV980 a change, that can only be made by Schneider Electric Services, may be required.
Contact Drives Technical Support at 888-SquareD or 888-778-2733.