Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which encoder card for Altivar ATV71 Frequency inverter drives are compatible with sincos encoder?
The only encoder card for ATV71 compatible with sincos encoder is VW3A3409.
Nevertheless, this encoder card cannot be placed in standard ATV71 drive. You have to use ATV71...S383 version (version that could control asynchronous or synchronous motors).
ATV71...S383 is not commercialized, unfortunately, therefore it makes sense to upgrade original assembly to ATV930+ analog encoder card.
FYI, attached is the catalog with encoder cards for ATV71.

Schneider Electric Saudi Arabia

Attachment(s)
altivar71optionsencoderinterfacecards_characteristicsreferencespresentation_en4.1_60285.pdf [73.06 KB]