Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Lonworks communication options are available on the ATV630 and ATV930 Process drives?
Issue:
Is Lonworks available on the ATV630 and ATV930 drives?

Product Line:
ATV630 and ATV930 drives.

Environment:
All

Cause:
Available options

Resolution:
The ATV630 and ATV930 drives do not currently have an option for Lonworks.  If you need to use Lonworks on the ATV630 and ATV930 drives you need to add a third party gateway.