Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the thresholds for PTC sensor open circuit, shortcircuit, overtemperature if connected to ATV600 option card?
If you use PTC sensor there is no configurable warning or fault threshold. The thresholds are fixed:
open circuit (R>100 kOhms)
short circuit (R<50 Ohms)
overheating (R>3 kOhm)
Moreover warning and fault comes at the same time. See attached page from option card manual. I added warning codes and fault codes (underlined), just replace x by 5 if your sensor is on AI5.

But if you use PT100 or PT1000, then you can configure parameters for warning and fault threshold. See attached screen from somove, parameters THxA for warning and THxF for fault with associated addresses. Actual temperature can be read from THxV.

Schneider Electric Saudi Arabia

Attachment(s)
Thermal monitoring1.jpg [262.65 KB]
Extracted pages from VW3A3203 IS_Extension_module_IO_EAV76404_00.pdf [148.85 KB]