How can we help you today?

Parameters List for Protocol EtherNet / IP of my ATV9xx DTM is not fully displayed on Ecostruxure Control Expert V14.0

With Ecostruxure Control Expert V14.0 opening ATV9xx DTMs configuration screen and going on screen Parameters List / Fieldbus / Port – Modbus TCP / EthernetIP / Protocol & Drive Profiles, we can see as it is highlighted below that main part of this screen is missing.

Control Expert V14.0



Unity Pro V13.1


Consequences:
Users will not be able to configure the connection parameters shown below.
But if these parameters are not visible and configurable these parameters by default are effective.
For thus that import an Unity Pro V13.1 application the effective parameters will be thus imported.

Note:
This is a known issue and a specific Control Expert HF will be published soon, ControlExpert_V140_HF0507345R.