Issue:
Fault history access on an ATV12 Drive
Product Line:
Altivar 12
Environment:
All
Cause:
N/A
Resolution:
Go into Menu Mon-, MAI-, and enter on dP1, dP2, dP3, and dP4 for the last 4 fault codes.
dP1 is the most recent fault.
dP4 is the oldest fault.
EP1, EP2, EP3, EP4 are the state of the drive at detected fault, corresponding to the fault number.
Fault history access on an ATV12 Drive
Product Line:
Altivar 12
Environment:
All
Cause:
N/A
Resolution:
Go into Menu Mon-, MAI-, and enter on dP1, dP2, dP3, and dP4 for the last 4 fault codes.
dP1 is the most recent fault.
dP4 is the oldest fault.
EP1, EP2, EP3, EP4 are the state of the drive at detected fault, corresponding to the fault number.
Released for: Schneider Electric Saudi Arabia