Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider offer padlockable selector switches?
Issue:
Selector switch with padlock option

Product Line:
22 mm Push Buttons

Environment:
XB4 Selector Switches

Resolution:
The ZB4 series has padlock option.
See the attached catalog section with various options in 2 and 3 positions selector switches.

Schneider Electric Saudi Arabia

Attachment(s)
selector switch padlockable.pdf [123.48 KB]