Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the TM2CSET terminal block connector set for Modicon M221 PLCs contain?

Issue

What does the TM2CSET terminal block connector set for Modicon M221 PLCs contain?

Product Line

Modicon M221 PLC

Environment

Physical connectors for wiring

Resolution

The TM2CSET terminal block connector set for the Modicon M221 I/O pins contains:

1x 8-pin screw connector terminal block

2x 10-pin screw connector terminal block

1x 12-pin screw connector terminal block

1x 13-pin screw connector terminal block

3x 9-pin screw connector terminal block


One set will include enough connector blocks of each type for each model of Modicon M221 PLC.