Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NOR returns an Offline status with a good 'DNP3' value and timestamp.

Issue
The quality status for a DNP3 variable is returned from the 'BMXNOR0200' as 'Offline' even though the DNP3 communications is confirmed to be
online and communicating.  When this occurs, the value for the DNP3 variable is returned with a good value and timestamp.


Product Line
BMXNOR0200 version 1.7, IR18

Environment
Windows 8, Windows 10


Resolution
The quality status for a DNP3 variable is returned from the 'BMXNOR0200' as 'Offline' even though the DNP3 communications is confirmed to be
online and communicating.  When this occurs, the value for the DNP3 variable is returned with a good value and timestamp.  This was found to
occur if the 'CPU Reg Mapping' of the DNP3 variable is configured with the flag selection.

asdfgh




The same issue will also occur if either the 'Default Static Variation' or 'Default Event Variation' are configured with the flag selection.

`123



The following workaround can be used to resolve the issue, if the DNP3 variable is defined as a DDT variable in the Unity application

  • Open an animation table.
  • Add the DDT variable to the animation table.
  • Expand the DDT variable.
  • Select the 'Flags' parameter.
  • Select the 'Modification' button to enable it.
  • Change the 'Flags' value from 0 to 1.

345

FAQ Applicable Conditions