Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a trial version of EcoStruxure Control Expert?

Article available in these languages: Spanish

Issue:

Is there a trial version of EcoStruxure Control Expert?

Product Line:

Control Expert

Resolution:

Control Expert comes with a 30 day trial license.

When the first installation is complete, the trial license is automatically activated during first launch of the software.

The trial license includes the maximum set of software product features which corresponds to the
Control Expert  XL package with M580  Safety Add-On.

If you do not activate your license within 30 days, Control Expert will no longer run once the trial period has expired.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)