Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can the Altistart ATS48 soft starter be wired up for the 2 wire run control to start the motor?

Issue:
2 Wire Control on ATS48

Product Line:
Altistart ATS48

Environment:
All

Cause:
Basic two-wire control

Resolution:
Wire the soft starters supplied +24vdc through your dry maintained contact back to the soft starters run and stop jumpered terminals.

See the ATS48 user manual for the terminal block connections.
https://www.se.com/us/en/download/document/1494409/


Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: