Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Altivar Process analog values be read over Ethernet if the inputs are not assigned?

Issue:
Is it possible to Read an Analog input status via Ethernet.

Product line:
Altivar Process 600 and 900 series

Resolution:
Yes, the values of the analog inputs can be read by checking the appropriate register values found in the Communication Parameters spreadsheet.  The analog input does not need to be assigned to any function.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)