{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot update OpenJDK version used by PowerChute Network Shutdown for Mac OS X using the Java Update feature

Issue:
Cannot update the Open JDK version using the Java Update feature in the About Box.

Product:
PowerChute Network Shutdown v4.3

Environment:
PowerChute v4.3, Mac OSX

Solution:

To change the version of OpenJDK used by PowerChute after updating the JDK you must uninstall PowerChute and re-install after installing the required version of Open JDK.

NOTE: PowerChute Network Shutdown running on Mac OSX uses the system / pre-installed JDK. PowerChute for Mac OSX is not bundled with a JDK. For more information see the PowerChute installation guide attached.

Schneider Electric Saudi Arabia

Attachment(s)
PowerChute Network Shutdown 4.3 Installation Guide.pdf [4.14 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.