Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV320 offer an Extended IO card?

Article available in these languages: Japanese

Issue:
Extended IO Card for ATV320.

Product line:
Altivar 320 Machine drive

Environment:
all

Cause:
Customer needs additional Inputs and Outputs.

Resolution:
No, the ATV320 does not offer an extended IO Card.  Consider the ATV340, ATV630 or ATV930 drives which do have an extended IO option.