Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the dissipated heat rating for ATV930 drives?
Issue:
Dissipated heat rating for ATV930 drives.

Product Line:
Altivar 930

Environment:
All

Cause:
Heat loss

Resolution:
Dissipated Heat Ratings

The first value is the power dissipated at a nominal current in the forced-cooled area of the drive.  The second value is the power dissipated at nominal current in the naturally cooled area, the value used in case of installation using the flush-mounting kit, separate hot and control part in the cabinet.  If the drive is installed in a standard cabinet, the sum of both values is to be taken into account.