Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On the ATV320 can motor rotation be reversed using programming?
Issue:
ATV320 reverse motor rotation with programming.

Product Line:
Altivar 320

Environment:
All

Cause:
Need to reverse motor rotation

Resolution:
No, the ATV320 does not have this functionality in the programming. Two motor leads will need to be swapped in order to reverse motor rotation.