Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the DI1 assignment show 'Not assigned' for both DI1 low or DI1 high in IO Map?

Issue:
DI1 assignment in IO Map saying not assigned for both DI1 low or DI1 high.

Product Line:
ATV600, ATV900

Environment:
All

Cause:
Customer checked DI1 assignment in I/O Map but didn't see DI1 current assignment 'Forward'.

Resolution:
Check menu 5.5 (Command and Reference), and Control Mode to see if it is set to "I/O profile", DI1 assignment only show "Forward" if the control mode is set to "Not Separate" or "Separate".