Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a competitive cross for Cutler Hammer 92-01943-01?
Issue:
Looking for a replacement HMI with a physical keyboard to replace a Cutler Hammer 92-01943-01.

Product Line:
Magelis HMIGK

Resolution:
The competitive cross for the Cutler Hammer 92-01943-01 is the HMIGK2310. The HMIGK is programmed with Vijeo Designer V6.2 SP5.1 or higher.