Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I am using EcoStruxure Control Expert Version 14. If I Activated a license on a Virtual machine can I copy the virtual Machine or duplicate it.
Issue

A user copied the virtual machine and wanted to have / see duplication of the license.

Product Line

EcoStruxure Control Expert V14 ( formerly known as Unity Pro )

Environment

Windows 10, 64 Bit used for Virtual Machine

Resolution

Copying of Virtual machine doesn't mean to duplicate the License for Ecostruxure Control Expert: Activation Id will not be duplicated.
You must transfer the license from initial VM to the new VM as you would do for a computer.
You need to send the license  to Schneider Electric License Server, Once the license is successfully sent, you can use the activation ID
for a another computer.