Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an HCF [Boards Compatibility] fault on an ATV340 series drive?
Issue:
HCF [boards Compatibility] fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
The [Pairing password] PPi parameter has been enabled and an option module has been changed.

Resolution:
Refit the original option module.
Confirm the configuration by entering the [Pairing password] PPI if the module was changed
deliberately.