How can we help you today?

BMXDDM3202K pin out diagram detail

Issue

This document provides additional clarity regarding the BMXDDM3202K 40 pin wiring diagram found in the Modicon X80 Discrete Input/Output Modules User Manual.

Product Line

BMXDDM3202K - a 24 VDC discrete 16 input/16 output IO module.

Resolution

Details added to diagram:
1. Orientation of the 40 pin male connector
2. Identification of pin numbers on the connector
3. External power supply + and - pin connections
4. Pin out numbers of the IO points (shown in red)

img1